cancel
Showing results for 
Search instead for 
Did you mean: 

IIS2MDCTR temperature rating.

HTaka.8
Associate

Please present the junction temperature rating of IIS2MDCTR,

Is it generally the same as the storage temperature?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @HTaka.8​ , please check if I well interpreted you question. The IIS2MDCTR max supply is 3.6V and max current (high performance mode, max ODR) is 1130uA, so the power consumed in the worst case is P=V*I=4mW. If you consider that the device package thermal resistance is 80°C/W, the thermal difference between the device and the environment is DeltaT=0.3°C worst case. Moreover, no worry about the junction temperature with respect to storage temperature. Regards