cancel
Showing results for 
Search instead for 
Did you mean: 

I need to measure an angle up to 30 degree with an accuracy of 0.1 deg. Is something like this possible with this new inclinometer?

Pasi MYLLYMAKI
ST Employee
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Carlo LARGHI
Associate III

the answer to this question is not straightforward, it really depends on which are the boundary conditions of your application (like the temperature range, the way you can use the axes of the inclinometer, the kind of calibration that you could afford to perform in your production line, etc).

Selecting IIS2ICLX, you have for sure the best MEMS inclinometer available to reach your accuracy target. 

View solution in original post

1 REPLY 1
Carlo LARGHI
Associate III

the answer to this question is not straightforward, it really depends on which are the boundary conditions of your application (like the temperature range, the way you can use the axes of the inclinometer, the kind of calibration that you could afford to perform in your production line, etc).

Selecting IIS2ICLX, you have for sure the best MEMS inclinometer available to reach your accuracy target.