2018-11-01 4:55 AM
Hello and thank you in advance,
i am trying to connect the LSM6DS3 accel+gyr with the 3110 magnetometer. I want to connect the mag on the LSM6DS3 and i want it to see it as an exterrnal sensor so i can sent the data of the magnetometer to LSM6DS3's internal FIFO. The problem is that in the LSM6DS3's datasheet there are this registers:
- SLV0_ADD -> (I2C slave address of the first external sensor (Sensor1) register (r/w)) // Magnetometer's slave address (everything ok)
- SLV0_SUBADD -> (Address of register on the first external sensor (Sensor1) register (r/w)) // This is an 8-bit register, what should i put here? Which register? The mag's register for only the x axis is 16-bit long -> OUT_X_MSB(8-bit) & OUT_X_LSB(8-bit)
Thanks
2018-11-01 6:13 AM
In the SLV0_SUBADD you should put the first address of the MAG3113 output register. In the SLAVE0_CONFIG register you should set how many consecutive reading operations should be performed to real all output data from external sensor.
Please read application note AN 4650:
2018-11-07 4:33 AM
Hello, i have read tha AN4650 before but i couldn't figure out what in two lines you clearly explained to me, thank you very much, i haven't tried it yet but i will.
2018-12-06 10:08 AM
Hello again,
i have an additional question,If i want to use the PASS_THROUGH_MODE, after i enable pass through do i treat the registers as if i was directly connected to it via I2C. Do i write and read registers directly?
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.