2015-06-02 9:20 AM
I have an application using the LIS3DH. I need to read the values from the on chip Temperature Sensor. I have properly setup the ADC_PD and TEMP_EN bit in the TEMP_CFG_REF (1Fh). I'm reading the OUT_3_L (0Ch) and OUT_3_H (0Dh) at an ODR of 50 Hz. The OUT_3_L seems to be random while OUT_3_H looks like valid data. Three different chips measure (OUT_3_H) as follows FA, F6 and FE. This translates to -6, -9 and -2. The Datasheet describes the TSDr as Temperature sensor output change vs temperature with a resolution of 1 digital/C. So my assumption is that the translated values of -6, -9 and -2 are delta (changes) from some reference temperature (possible at MFG calibration). The ambient temperature in the room is 23 C (~73 F). My assumption per Datasheet was that the reference temperature is 25 C but this only correlated to the 3rd value. Is there a reference temperature that is different in each chip? Is there a way to access this reference temperature? Possible in one of the reserved addresses?
Thank you,
#temperature-sensor #lis3dh2017-10-26 6:25 PM
Presumably because the accuracy of the measurements is effected by temperature.
2018-03-24 5:04 AM
The problem is that it is absolutely not described as such in the datasheet and is very vague for the use of it.
I spend hours to understand why this would act in a such way, lucky that some of you guys talked about this matter.
I finally understood and see that all I was doing worked properly.
I would add that it is one of the worse datasheet I ever had to read.
Thanks guys for your help
2024-02-06 11:39 PM
For me it was showing Temperature: -253, How to consider