2019-08-18 5:41 PM
Hi there.
We tried to get data from the LSM6DS3 at maximum speed but data rate of the sensor was always around 400Hz.
Datasheet say 'LSM6DS3 supports up to 6.66kHz'. Then, can I read the raw data at 6.66kHz through SPI communication?
If it is possible, which resistor or setting must be configured?
Our code is down below.
Firstly, initializing LSM6DS3
void lsm6ds3_init(void)
{
// CTRL1_XL Write
TxData[0] = 0x10; // address
TxData[1] = 0x00; // power down
HAL_SPI_Transmit(&hspi1,&TxData[0],1,0xff);
HAL_SPI_Transmit(&hspi1,&TxData[1],1,0xff);
uint8_t cmd=0x10 ;
uint8_t ret=SPI_Read(cmd,1,10);
TxData[0] = 0x15; // address
TxData[1] = 0x00; // highperformance mode
HAL_SPI_Transmit(&hspi1,&TxData[0],1,0xff);
HAL_SPI_Transmit(&hspi1,&TxData[1],1,0xff);
cmd=0x15 ;
ret=SPI_Read(cmd,1,10);
//CTRL1_XL
TxData[0] = 0x10; //address
TxData[1] = 0xA0; // value 1010 00 00
cmd=0x10 ;
ret=SPI_Read(cmd,1,10);
HAL_SPI_Transmit(&hspi1,&TxData[0],1,0xff);
HAL_SPI_Transmit(&hspi1,&TxData[1],1,0xff);
// CTRL2_G_XL Write
TxData[0] = 0x11; //address
TxData[1] = 0x80; //value
cmd=0x11 ;
ret=SPI_Read(cmd,1,10);
HAL_SPI_Transmit(&hspi1,&TxData[0],1,0xff);
HAL_SPI_Transmit(&hspi1,&TxData[1],1,0xff);
}Secondly, Getting raw data from the sensor
while(1){
LSM6DS3_state=LSM6DS3_Read_Status();
if(LSM6DS3_state&0x01){
SensorData[2]=LSM6DS3_ReadXLData(0);
SensorData[3]=LSM6DS3_ReadXLData(1);
SensorData[4]=LSM6DS3_ReadXLData(2);
SensorData[5]=LSM6DS3_ReadXLData(3);
SensorData[6]=LSM6DS3_ReadXLData(4);
SensorData[7]=LSM6DS3_ReadXLData(5);
SnsorData[8]=LSM6DS3_ReadGData(0);
SensorData[9]=LSM6DS3_ReadGData(1);
SensorData[10]=LSM6DS3_ReadGData(2);
SensorData[11]=LSM6DS3_ReadGData(3);
SensorData[12]=LSM6DS3_ReadGData(4);
SensorData[13]=LSM6DS3_ReadGData(5);
}
}