2019-02-28 9:50 AM
Latest (6.x) release does not support my existing boards and I need to keep these running.
2019-03-07 2:16 AM
Hi Bill, you can download X-CUBE-MEMS1 (V4.4.1) at this link:
https://www.st.com/en/embedded-software/x-cube-mems1-v4.html
HOwever, I suggest you to upgrade the X-NUCLEO-IKS01A1 to the last X-NUCLEO-IKS01A3 which includes the interface for the last ST sensors
Regards
2019-03-07 12:19 PM
Hi, Thank you! I will download these.
I did try to order the A3 but it is not ready for sale. I ordered the A2 and it works.
Regards
Bill
2019-03-08 12:32 AM
yes, it will be available soon!
regards