2020-08-31 1:27 AM
Hello ST community,
I was going through the application note for LIS2DS12 (https://www.st.com/resource/en/application_note/dm00218428-lis2ds12-alwayson-3d-accelerometer-stmicroelectronics.pdf) which mentions in section 5.9.1 that STEP_COUNT_DELTA can be configured to generate interrupt if a step is detected in a certain time period. Does configuration of this register also apply to the step count value in STEP_COUNTER register?
Regards,
Anusha
Solved! Go to Solution.
2020-09-01 6:14 AM
Hi Anusha @AB.4 ,
the step counter register only tracks the number of steps detected until it is reset (RST_nSTEP bit of reg STEP_COUNTER_MINTHS (3Ah) set to 1).
So: no, the STEP_COUNT_DELTA configuration does not affect the STEP_COUNTER register.
2020-09-01 6:14 AM
Hi Anusha @AB.4 ,
the step counter register only tracks the number of steps detected until it is reset (RST_nSTEP bit of reg STEP_COUNTER_MINTHS (3Ah) set to 1).
So: no, the STEP_COUNT_DELTA configuration does not affect the STEP_COUNTER register.
2020-09-01 7:19 AM
Hi Niccolo,
Thanks for your response. This is clear.
Regards,
Anusha