cancel
Showing results for 
Search instead for 
Did you mean: 

Do you have also another real life example for FSM in sensors? Is the interval data split the only application? Any others apps?

Pasi MYLLYMAKI
ST Employee
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Carlo LARGHI
Associate III

there are many examples, you can refer to Github repository highlighted in webinar material for some. In particular, in the context of the IIS2ICLX, the mentioned application for monitoring the traffic load on a bridge rely on combined usage of FSM and MLC

The other example showed in the webinar is the direct angle output from inclinometer based on MLC classification. With other ST sensors with MLC, we have also examples of detecting if drilling machine is idle, tightening screw or drilling to wood etc, this type of example could then be extended to automated machinery and this example can be for sure adapted also to run on IIS2ICLX.

View solution in original post

1 REPLY 1
Carlo LARGHI
Associate III

there are many examples, you can refer to Github repository highlighted in webinar material for some. In particular, in the context of the IIS2ICLX, the mentioned application for monitoring the traffic load on a bridge rely on combined usage of FSM and MLC

The other example showed in the webinar is the direct angle output from inclinometer based on MLC classification. With other ST sensors with MLC, we have also examples of detecting if drilling machine is idle, tightening screw or drilling to wood etc, this type of example could then be extended to automated machinery and this example can be for sure adapted also to run on IIS2ICLX.