cancel
Showing results for 
Search instead for 
Did you mean: 

Can the functionality (0,1) of the sensortile.box LED's be implemented into the algobuilder using the functional block creator? If this is possible can you provide an example.

J-Damron
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Miroslav BATEK
ST Employee

Hello,

yes, it can be done. In attachment is simple example with LED function block. The input controls the LED2 (green LED) on SensorTile.box. If the input is equal to 1 the LED is on, otherwise is off. You can place the file to c:\Users\USER_NAME\STMicroelectronics\AlgoBuilder\Library\ directory, then is should be visible in AlgoBuilder application.

View solution in original post

2 REPLIES 2
Miroslav BATEK
ST Employee

Hello,

yes, it can be done. In attachment is simple example with LED function block. The input controls the LED2 (green LED) on SensorTile.box. If the input is equal to 1 the LED is on, otherwise is off. You can place the file to c:\Users\USER_NAME\STMicroelectronics\AlgoBuilder\Library\ directory, then is should be visible in AlgoBuilder application.

J-Damron
Associate II

Thank you again Miroslav!