2018-04-09 5:30 AM
Hey,
I'm testing the way BlueCoin is working with FP-AUD-SMARTMIC1 distribution. I used this guide to connect and start working:
The problem is: when I try to start a session with the tool available in this distribution (GUI or CLI), it fails with a ping error, even though the com port i'm using is available and seeable. Does anyone have any ideas here?
Also Online Support of ST is not working (cookies problem ) - is there any other way to get support from ST?
Thanks ,
Natasha
#smartmic1-distribution #bluecoin2018-09-26 12:14 AM
Hello Natasha,
I am dealing with the same problem.
When I run the CLI distribution on my PC, it works fine.
However, on my RasPi 2 and Jetson TX2, it stops at ping error.
Have you made it work yet?
Thanks,
Trung.
2018-10-01 2:31 AM
Hi Natasha.
I run the script from https://stackoverflow.com/questions/47480214/connect-usb-scale-in-ubuntu-cdc-acm-says-failed-to-set-dtr-trs
And it works.
Hope it help.
Thanks,
Trung.