cancel
Showing results for 
Search instead for 
Did you mean: 

Accelerometers, 2g, low noise < 100 μg, I2C with SA0 and SA1 to connect 4 devices

JJońs.1
Associate II

I am looking for accelerometer ultra low noise with low g.

I want to connect 4 sensors using I2C, so I need 2 pin SA0 and SA1.

Do you have such sensors

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
JWu.12
Associate III

Hi, from my experience there isn't, if you want to connect multiple devices you need to use the SPI lines.

Otherwise, if you don't need to acquire signals simultaneously, you can use one of the accelerometers (for example the LIS2DW12) and read first from two of them, keeping the CS of the other two high and writing the I2C_DISABLE bit of the CTRL2 (21h) register to 1, in order to disable the I2C block. But I guess this is not the best solution ever.

https://www.st.com/resource/en/datasheet/lis2dw12.pdf

View solution in original post

3 REPLIES 3
JWu.12
Associate III

Hi, from my experience there isn't, if you want to connect multiple devices you need to use the SPI lines.

Otherwise, if you don't need to acquire signals simultaneously, you can use one of the accelerometers (for example the LIS2DW12) and read first from two of them, keeping the CS of the other two high and writing the I2C_DISABLE bit of the CTRL2 (21h) register to 1, in order to disable the I2C block. But I guess this is not the best solution ever.

https://www.st.com/resource/en/datasheet/lis2dw12.pdf

OK, thank you for your answer.
I have one more question. So far I used accelerometer NXP FXLS8471Q (end of life) 14 bits. Do you have accelerometer LLGA16 (3x3x1mm) which is 14 or 16 bits. LIS331DLH and LIS3DH looks good, the same footprint but only 12 bits

Regards,
Janusz Jonski

Hi Janusz, for effective 14 or 16 bit resolution I believe you have to change package into the LIS2DW12, for example.

There was the LIS3DSH satisfying your requirements, but I believe it is nrnd now.