• Images in Profile (mƎALLEm)
  • My Images for mƎALLEm

My Images for mƎALLEm

  • Albums
  • All Images
Image Options
  • Flag Image for Review
  • Bookmark
  • Subscribe to RSS Feed

Album: Profile (mƎALLEm)

by mƎALLEm
Figure 1. Block diagram
Figure 2. NUCLEO-H753ZI: STLINK crystal oscillator of 25 MHz
Figure 3. NUCLEO-H563ZI: STLINK crystal of 24 MHz
Figure 4. Using ST-LINK firmware upgrade tool to modify the MCO frequency
Figure 5. Using STM32CubeProgrammer tool to modify the MCO frequency
Figure 6. Using STM32CubeMx tool to set the right RCC configuration
SofLit_0-1727103726255.png
SofLit_0-1726223170325.png
SofLit_0-1727103726255.png
CM4_disable.png
1.png
SofLit_0-1729078448084.png
SofLit_0-1729078448084.png
CAN_bus_structure.png
schematics.png
SofLit_0-1734613369887.png
message.png
scope_0.png
Figure 1. Exporting option bytes in the “OB” menu
Figure 2. Saving the option bytes file config
Figure 3. Importing option bytes in “OB” menu
Figure 4. Opening the option bytes file config
Figure 5. Applying the new option bytes config (factory values)
Figure 6. Using “Reset MCU to Factory Settings” option
Figure 7. Applying the option factory settings
Figure 8. Waiting for the operations to complete
CM7_CM4_Gated.png
CM7_CM4_Gated.png
Figure 1. Start a project based on a ST board
Figure 2. Select NUCLEO-F103RB
Figure 3. Click yes to initialize the peripherals
Figure 4. Default pinout view
Figure 5. CAN activation
Figure 6. CAN pins activated
Figure 7. CAN pins on the board are free
Figure 8. CAN in Loop Back mode
Figure 9. Configuring CAN in Loop Back mode
Figure 10. Basic CAN parameters setting
Figure 11. The CAN clock is on APB1 domain
Figure 12. System clock configuration
Figure 13. Default CAN timing configuration in STM32CubeMX
Figure 14. CAN timing configuration
Figure 15. Setting the pull-up on CAN_Rx pin
Figure 16. Enable CAN RX0 NVIC interrupt channel
Figure 17. Project code generation
Figure 18. Project explorer view after generating the code
Figure 19. Compile the project
Figure 20. Configure the Saleae logic analyzer digital channel 0 input in CAN mode
Figure 21. CAN configuration with Saleae logic analyzer
Figure 22. Start a debug session of the application in STM32CubeIDE
CM7_CM4_Gated.png
Previous
CM7_CM4_Gated.png
Next
Added ‎2025-02-06 5:20 AM