cancel
Showing results for 
Search instead for 
Did you mean: 

Where could I find the BOM of components in Fig. 4 of the S2-LP datasheet? There are different passive components like L7, C21 and C16 using the S2-LP in combination to BALF-SPI2-02D3 for 433MHz. And knowing the values would reduce the time of design.

JInve.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Cyril BLARD
ST Employee

Hi, we suggest you to use L7: 100nH (LQG reference as example), C21 & C216=100pF used only to DC cut.

View solution in original post

1 REPLY 1
Cyril BLARD
ST Employee

Hi, we suggest you to use L7: 100nH (LQG reference as example), C21 & C216=100pF used only to DC cut.