2019-04-21 6:03 PM
I'm trying to get the discovery board to play a wav file that I've converted to an array of 16b hex values. So far, I have only been able to output an obnoxious noise.
I have tried keeping the registered in the CS43L22 all at default.
I have tried configuring the beep to ensure that the uC is talking properly but the beep isn't working either.
Does anyone have any experience getting this working with the new HAL libs and where I might have gone wrong?
Sample command to enable the CS43L22. Do I have the address and data in the right order for the HAL_I2C_Master_Transmit function?
audioControl [0] = 0x02;
audioControl [1] = 0x9E;
if(HAL_I2C_Master_Transmit(&hi2c1,0x94,audioControl,2,50) != HAL_OK)
{
HAL_GPIO_WritePin(GPIOD, LD5_Pin, GPIO_PIN_SET);
}I2C Config
hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 100000;
hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c1.Init.OwnAddress1 = 0;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}I2S Config
hi2s3.Instance = SPI3;
hi2s3.Init.Mode = I2S_MODE_MASTER_TX;
hi2s3.Init.Standard = I2S_STANDARD_MSB;
hi2s3.Init.DataFormat = I2S_DATAFORMAT_16B;
hi2s3.Init.MCLKOutput = I2S_MCLKOUTPUT_ENABLE;
hi2s3.Init.AudioFreq = I2S_AUDIOFREQ_44K;
hi2s3.Init.CPOL = I2S_CPOL_LOW;
hi2s3.Init.ClockSource = I2S_CLOCK_PLL;
hi2s3.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_DISABLE;
if (HAL_I2S_Init(&hi2s3) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}