cancel
Showing results for 
Search instead for 
Did you mean: 

What can I do to solve Data mistake on SPWF01SA.11?

Jean DEMBEGA
Associate II
Posted on June 12, 2017 at 17:05

none

#tls-spwf01sa.11 #data-lost #large-data #spwf01sa.11
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Gerardo GALLUCCI
ST Employee
Posted on June 12, 2017 at 17:40

Hi Jean,

problem is that, if you want to receive X bytes, you need to store (in worst case) 2X bytes. Record is not decrypted if it's not fully received. There is an alloc/realloc mechanism inside.

Module has 64KB RAM to run everything, including filesystem (if any), TLS (if used), webserver (if clients are in), etc. Check 'AT+S.STS=free_heap' after WIND:24.

Basically, using a standard SPWF01S FW, cannot receive all of this amount of data over TLS. Use HTTP1.1 header capability to ask for smaller chuncks (Content-Length / Content-Range). Ask for a customization to your ST distributor/reference.

Alternative option: move to SPWF04S

jerry