cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF01S in MiniAP Mode with WEP Security

Clara Antoine
Associate
Posted on June 12, 2017 at 16:30

Hello,

I configured my SPWF01S in miniAP Mode just like this:

# Dumping All Configuration Keys:

# nv_manuf = ST

# nv_model = SPWF01S

# nv_serial = value

# nv_wifi_macaddr = 00:80:E1:B8:6A:CC

# etf_mode = 0

# blink_led = 1

# wind_off_low = 0x00000000

# wind_off_medium = 0x00000000

# wind_off_high = 0x00000000

# user_desc = anonymous

# escape_seq = at+s.

# localecho1 = 0

# console1_speed = 115200

# console1_hwfc = 0

# console1_enabled = 1

# console1_delimiter = 0x0000002C

# console1_errs = 1

# sleep_enabled = 0

# standby_enabled = 0

# standby_time = 10

# wifi_tx_msdu_lifetime = 0

# wifi_rx_msdu_lifetime = 0

# wifi_operational_mode = 0x00000011

# wifi_beacon_wakeup = 1

# wifi_beacon_interval = 100

# wifi_listen_interval = 0

# wifi_rts_threshold = 3000

# wifi_ssid = 52:48:45:41:2D:54:49:54:41:4E:2D:4E:45:54:57:4F:52:4B:00:00:00:00:00:00:00:00:00:00:00:00:00:00

# wifi_ssid_len = 18

# wifi_txfail_thresh = 5

# wifi_ht_mode = 0

# wifi_channelnum = 6

# wifi_opr_rate_mask = 0x00003FCF

# wifi_bas_rate_mask = 0x0000000F

# wifi_mode = 3

# wifi_region = 1

# wifi_auth_type = 0

# wifi_atim_window = 0

# wifi_powersave = 0

# wifi_tx_power = 18

# wifi_rssi_thresh = 0

# wifi_rssi_hyst = 0

# wifi_ap_idle_timeout = 120

# wifi_beacon_loss_thresh = 10

# wifi_priv_mode = 1

# wifi_wep_keys[0] = 41:42:43:44:45:00:00:00:00:00:00:00:00:00:00:00

# wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

# wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

# wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

# wifi_wep_key_lens = 05:00:00:00

# wifi_wep_default_key = 0

# wifi_wpa_psk_raw = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

# wifi_wpa_psk_text =

# ip_use_dhcp = 1

# ip_use_httpd = 1

# ip_mtu = 1500

# ip_hostname = iwm-B8-6A-CC

# ip_apdomainname = captiveportal.net

# ip_apredirect = firstset.html

# ip_ipaddr = 192.168.0.50

# ip_netmask = 255.255.255.0

# ip_gw = 192.168.0.1

# ip_dns = 192.168.0.1

# ip_http_get_recv_timeout = 3000

# ip_wait_timeout = 12000

# ip_dhcp_timeout = 20

# ip_sockd_timeout = 250

# ip_dhcp_lease_time = 120

# ip_dns_mode = 0

# ip_use_cgis = 0x0000000F

# ip_use_ssis = 0x0000000F

# ip_use_decoder = 0x00000000

I then try to connect an Android mobile phone to the AP. When I enter the wrong password, it is not working (hopefully). However when I enter the right password, it connects but I get this error:

+WIND:45:Dot11 AuthIllegal 25641/164

I saw that the first number should be a 0 or a 1.

Surprisingly, when connected I can exchange data through a socket between the 2 devices. So I don't understand where this error comes from..

Do you have any idea ?

Thanks,

Kind regards,

Clara

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Gerardo GALLUCCI
ST Employee
Posted on June 12, 2017 at 17:15

Ciao Clara,

it's not a real error (you can ignore it. change wind_off_* variable)

Try to change the authentication method. 

wifi_auth_type. from 0 (open) to 1 (shared). Any difference?

j

Clara Antoine
Associate
Posted on June 12, 2017 at 17:22

Hello,

That is what I thought but I wasn't sure, thank you !

I tried changing wifi_auth_type but it didn't change anything..

Thank you for your fast answer !

Regards,

Clara