cancel
Showing results for 
Search instead for 
Did you mean: 

STUSB4700 : Sourcing only when external power is available, product drawing from Vbus otherwise

gwentech
Associate

I'm hoping to use the STUSB4700 in a product design.  The product needs to be supplied by normally by a tablet (only 5V @ 100mA required).  Sometimes the product will have external power available and when it does, I want to source power to the tablet.  Understanding the STUSB4700 is not a dual role, can I simply draw from Vbus for the sink scenario and then when external power is available, the STUSB4700 jumps into action and negotiates sourcing?

Ref page 21 application example of datasheet.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
gwentech
Associate

Looks like no support is available here...?