cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-FKI433V2 send custom data on GPIO

SimoMass88
Associate

Hi, I'm new with this development board.

My target is to use the S2-LP DK Application to configure the board to send data from a GPIO.

Do I have to put my data on GPIO_0 and the clock signal to GPIO_1?

Why is the clock signal needed?

In this way it is possible to change also the modulation? For example I want to send my packet on OOK mode or FSK mode.

 

Thanks

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0