2024-12-13 9:36 AM
Hello everyone,
I am currently working with the SKA2DHV module based on the ST60 and I’m facing some difficulties in finding detailed information about it, especially regarding the interface specifications. The documentation mentions the need for an SGMII interface, but I am unable to find additional details that would help clarify how to properly implement it.
I was wondering if anyone here has experience working with the ST60A2G and could provide more insight into its usage or share any resources that could help.
Additionally, I am considering using the DP83869HM transceiver from Texas Instruments, which is designed specifically for the SGMII interface mentioned in the documentation. Based on its specifications, do you think the DP83869HM would be compatible with the ST60A2G module?
Any advice or suggestions would be greatly appreciated!
Thank you in advance.
2025-02-03 12:25 PM
Welcome @dpereztol, to the community!
I have just come across your older question: the data of all ST60 devices is strictly confidential and will only be handed over if an NDA is signed. For this reason, nobody in the public community will be able to help you, so you should contact your local ST contact.
Hope that helps?
Regards
/Peter