cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF04SA no longer communicates

Lorenzo Pecci
Associate II
Posted on July 03, 2017 at 17:35

I'm using the X-NUCLEO-IDW04A1. After a restart, the module no longer communicates via serial port (UART).

LED3 (Red - GPIO14) is On.

The 'MicroPython_mode' (pull_up GPIO8) at reboot work fine.

How can I restore the module?

#spwf04sa #comunication #idw04a1
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Elio Cometti
Senior II
Posted on July 03, 2017 at 23:05

You can restore the factory configuration by resetting the board with GPIO0 (J2 pin 4) pulled up.

Posted on July 04, 2017 at 10:27

Yes, thanks, but doesn't work. Still silent.