cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF01SA1 http connection drops while accessing RAM file

rishi2
Associate III
Posted on September 19, 2017 at 16:26

I am using SPWF01SA (ver :160129-c5bf5ce-SPWF01S) with CubeExpansion_WIFI1_V3.0.2 with custom hardware.

Trying a simple test of adding a html file to RAM using wifi_file_create(). File is added as i confirmed this with wifi_file_list(). I am starting the module in miniAP mode and when i try to access this html file from wifi client laptop, http connection drops. But if i try to access any other html file i can get it in my browser. 

//code for file creation and module startup....

WiFi_Status_t status = WiFi_MODULE_SUCCESS;

uint8_t ssid[11] = {'R','L','C','_','C','O','N','F','I','G',0};

uint8_t tmp[85];

sprintf((char*)tmp,'%s','<!DOCTYPE html><html><head><title>testpage</title></head><body>testpage</body></html>');

InitWiFi_GPIO();

StartWiFiHardware();

status = SET_Configuration_Addr(WIFI_IP_APDOMAINNAME, 'domain.net');

if(status != WiFi_MODULE_SUCCESS)

   LOG('failed to set domain name...\n');

wifi_ap_start(ssid,6);

status = wifi_file_create('test.html',sizeof(tmp),(char*)tmp);

if(status != WiFi_MODULE_SUCCESS)

   LOG('failed to create file...\n');

else

   LOG('file created...\n');

status = wifi_file_list();

 wifi_file_show((uint8_t*)'test.html');

while(1){};

///// Output from teraterm log window

Initializing SPWF01SA1 Interface..

+WIND:1:Poweron (160129-c5bf5ce-SPWF01S)

+WIND:13:ST SPWF01S IWM: Copyright (c) 2012-2015 STMicroelectronics, Inc. All rights Reserved.

+WIND:3:Watchdog Running

+WIND:0:Console active

+WIND:32:WiFi Hardware Started

WiFi Module started...

+WIND:26:WiFi Started AP with network 'RLC_CONFIG'

+WIND:24:WiFi Up:172.24.62.1

Connected to network now, ready for TCP communication ...

>>Soft Reset Wi-Fi module

+WIND:2:Reset

+WIND:1:Poweron (160129-c5bf5ce-SPWF01S)

+WIND:13:ST SPWF01S IWM: Copyright (c) 2012-2015 STMicroelectronics, Inc. All rights Reserved.

+WIND:3:Watchdog Running

+WIND:0:Console active

+WIND:32:WiFi Hardware Started

WiFi Initialised and Ready..

file created...

+WIND:26:WiFi Started AP with network 'RLC_CONFIG'

+WIND:24:WiFi Up:172.24.62.1

OK

D 85 /test.html

I 461 /input_demo.shtml

I 384 /output_demo.html

I 614 /index.html

I 157 /peers.shtml

I 193 /config.shtml

I 180 /message.shtml

I 174 /status.shtml

I 5496 /remote.html

I 3447 /firstset.html

I 212 /404.html

OK

OK

<!DOCTYPE html><html><head><title>testpage</title></head><body>testpage</body></html>

OK

.....................

#spwf01sa1
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Elio Cometti
Senior II
Posted on April 24, 2018 at 15:16

Dear,

the file created by wifi_file_create() must include a complete HTTP response header plus the document content that will be delivered to the client.

Regards,

Elio