cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF01 : can't connect to the mini AP

marc Georgin
Associate II
Posted on January 04, 2017 at 09:52

Hello,

I'am using this module to connecte my borad to Internet. 

This module can create a mini AP so a user can connect its laptaop or smartphone to the SPWF01 and configure the WIFI connexion (SSID and pass).

I have no problème to connect to the mini AP with an old WIKO smartphone but I can't connect with a newer smartphone (Huawei P9 lite).

I have also discover a weird thing : If I first connect anything (old WIKO or laptop) to the mini AP, and then try with the P9 lite, it can connect to the mini AP.

thanks for your help.

Marc G

This discussion is locked. Please start a new topic to ask your question.
17 REPLIES 17
Gerardo GALLUCCI
ST Employee
Posted on January 05, 2017 at 16:18

Hi,

which version are you using?

Regards

Jerry

Posted on January 09, 2017 at 11:01

Hello,

thanks for your help, the version of the firmware of the SPWF01 is 3.4.

regards,

Marc

Posted on January 09, 2017 at 15:58

Hi Marc,

please use the latest FW 3.5. If problem is still there, we'll find a way to solve It. Unfortunatelly I have not that device to reproduce the issue. 

Thanks

j

Posted on January 12, 2017 at 10:43

Ok, I'll try the last firmware.

Posted on January 12, 2017 at 13:47

hello,

I can't easily change the firmware of the 

SPWF01 on my board. I receives a new edition of my board with, i guess, a newer firmware version for the SPWF01. Below are the tow version extracted from the UART log :

Older board : +WIND:1:Poweron (150410-c2e37a3-SPWF01S)

----> My P9 lite can't connect

Newer board : +WIND:1:Poweron (160129-c5bf5ce-SPWF01S) ----> My P9 lite can connect

Thanks to this test, I assumed that a firmware update of the OLD baord will solve the problem.

Can you confirm my analysis ?

Can you tell me which firmware 3.4 ou 3.5 are my too boards ?

Thanks for your help.

Marc 

Gerardo GALLUCCI
ST Employee
Posted on January 12, 2017 at 19:20

Hi Marc,

Jan 29th 2016 was FW3.5 ->

160129-c5bf5ce-SPWF01S

Apr 10th 2015 was FW3.4 -> 

150410-c2e37a3-SPWF01S

Let me know if I can consider closed this issue.

Thanks to you!

jerry

Posted on January 13, 2017 at 08:37

Thanks ! This issue can be closed

Gerardo GALLUCCI
ST Employee
Posted on January 13, 2017 at 11:18

Please use 'Mark Correct' button

marc Georgin
Associate II
Posted on February 08, 2017 at 14:30

Hello, 

I have solved my problem with my P9 lite phone with the newer firmware version of the module. But with an other smartphone (Nexus 5X android 7) I can' connect to the AP of the module. When I click on the SSID in the WIFI parameter, the smartphone connects to the AP for few seconds then deconnects then reconnects for a few seconds .... and so on. I am working with a module with firmware 3.5 (the last).

thanks for your help.

Marc