cancel
Showing results for 
Search instead for 
Did you mean: 

SPBTLE-1s Example Project Run

Altamash Abdul Rahim
Associate II

Hello,

I am evaluating SPBTLE-1s module. I am working on a example project provided by the BlueNRG-1_2 DK 3.1.0 (remote control). The project build on truestudio and is burned on chip via st link utility. Application success messages prints on the serial terminal but no module is discoverable on my android phone. I'm using BlueNrg android app.

Note: for Spbtle-1s i have changed the preprocessor macro from 16MHz external clock to 32MHz.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
alok
Senior

Kindly try another project like Beacon, which is simple to test