cancel
Showing results for 
Search instead for 
Did you mean: 

Library, Project and Utilities folders are not present in

CALVE
Associate II

Hi, I downloaded from my ST login the file "en.stsw-bluenrg1-dk.zip" and installed it. I don't found complete software directory structure as explain on "en.DM00298232.pdf" §6.1. Library, Project and Utilities folders are not present. Where can i download all it?

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Winfred LU
ST Employee

Please refer to the release notes.

file:///C:/Program%20Files%20(x86)/STMicroelectronics/BlueNRG-1_2%20DK%203.1.0/Docs/BlueNRG1_DK_release_notes/_release__v3_1_0.html

  • Library, Project, Utilities folders are located under {User} –> ST in order to be able to directly compile projects even with Windows User Account Control activated.