2018-11-21 9:58 AM
Hello,
I would like to design my own PCB for a Bluetooth Mesh project. Currently I am using STEVAL-IDB007V1 and STEVAL-IDB008V2 boards by configuring and provisioning them as mesh nodes through smartphone. I want to know whether it is required to program the STM32L151CBU6 microcontroller in order to use BlueNRG-1/2 in network coprocessor mode ?
In the documentation, it is mentioned that "In order to configure the BlueNRG-2 device as a network coprocessor, the device must be programmed with a specific application, named DTM (direct test mode). " Moreover , it is also mentioned that
"The STM32L microcontroller on the board is not intended to be programmed by users. ST provides a preprogrammed firmware image for the sole purpose of interfacing BlueNRG-1, BlueNRG-2 to a USB host device (e.g., a PC)."
So, I want to ask if I want to design my own PCB for BlueNRG-1/2, then is it required to program firstly the STM32L microcontroller with the DTM source code provided in SDK ? Kindly let me know the necessary steps.
2018-11-22 1:28 AM
@alok @STM Community ...Could you please help ?
2018-11-22 1:40 AM
Hi MH,
The BlueNRG-1, -2 can be used in 2 modes: Network coprocessor mode or Application processor
The comments you have mentioned are for Network co-processor mode. Because in this case the external controller (STM32) is needed.
For the Mesh firmware example you are using in STSW_BNRG-Mesh solution, the BlueNRG-1, 2 are used in Application mode. The device can work independently without a need of STM32
Hope it is clear
In addition, the STM32 available on the STEVAL-IDB007V1 and STEVAL-IDB008V2 boards is to provide the USB-UART bridge. Also, it provides functionality to drag-drop the binary file to program the BlueNRG-1, -2.
So, you can design your own hardware without any STM32L1
2018-11-22 2:16 AM
Hi Alok,
Thank you for reply. If I use only BlueNRG-1,2 without STM32L1, how can I program the output or binary files to BlueNRG-1,2 on my own hardware board ? What changes do I need to make to connections of BlueNRG-1,2 in schematic of STEVALIDB007V1 board ?
2018-11-22 2:29 AM
Hi MH,
You need the SWD connections. Refer to schematics for example for this design which is based on BlueNRG-2: STEVAL-BCN002V1B
Schematics are inside the Databrief:
https://www.st.com/resource/en/data_brief/steval-bcn002v1b.pdf
You will surely need a programming tool like ST-LINK/V2
2018-12-05 2:20 AM
Hi @alok ,
I tested the SWD connection to program BlueNRG-1,2 using ST Link/v2 and it worked. I want to further confirm that for programming mesh firmware on BlueNRG-1,2, there is no need of sheet 2 in this schematic and can I implement mesh firmware by using only sheet 1 and 3 of this schematic ?
2018-12-05 5:03 AM
Hi @alok ,
Can you also tell me the value of inductor "L5" used for both STEVAL-IDB007V2 and STEVAL-IDB008v2 ?
Its value is not mentioned either in schematic or BOM.
2018-12-05 5:49 AM
Hi MH,
In my opinion, L5 will depend on the recommendation of the XTAL used. You can leave the footprint for the bead
2018-12-05 12:04 PM
Hi ,
Can you let me know the values for both cases i.e. for 32MHz crystal (used in STEVAL-IDB008V2) and 16 MHz crystal (used in STEVAL-IDB007V2) ?
2018-12-05 12:05 PM
Hi @alok ,
Could you please reply to this question as well ?