cancel
Showing results for 
Search instead for 
Did you mean: 

How to customize the advertising packet?

dimitar
Associate II
Posted on January 09, 2015 at 18:46

Hi,

I'm trying to customize the advertising packet, but it's unsuccessful so far.

I use STEVAL-IDB002V1

BlueNRG HW v3.0

BlueNRG FW v6.4

Motherboard FW v1.4

Since the command ACI_GAP_SET_DISCOVARABLE doesn't give much options I've tried to use  HCI_LE_SET_ADVERTISING_PARAMETERS , HCI_LE_Set_Advertizing_Data, HCI_LE_SET_ADVERTISE_ENABLE.

The response to  HCI_LE_SET_ADVERTISING_PARAMETERS and HCI_LE_SET_ADVERTISE_ENABLE is Unknown HCI Command.

Are these supported commands?

Is there any other way to customize the advertising and scan packet?

Thanks

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
lucaleonardi.919
Associate II
Posted on January 05, 2016 at 11:15

Hi, I want use an X-NUCLEO-IDB05A1 on (STEVAL-IDB002V1) RF MOTHERBOARD (vers 3.0). How do you connect them?

Thanks

lucaleonardi.919
Associate II
Posted on January 22, 2016 at 11:43

Hi,

I need to use an X-NUCLEO-IDB05A1 on (STEVAL-IDB002V1) RF MOTHERBOARD (vers 3.0). Don't I may connect them with jumper cable male to female?

Using X-NUCLEO-IDB05A1 can I sending broadcast messages without the use of the advertisment? I need to have a device that send broadcast messages and observer the messages of the other device.

Thanks