How can i use a ISM43362-M3G-L44 wifi module as a hotspot using a stm32F451 Processor?
We are creating a board with both WIFI and bluetooth on it along with other sensors and communictions equipment. We have about 450m of data to transfer (4-8 hours of run time data) . BLE is out due to the amount of time to transfer the data. bluetooth classic is out because the developer creating the androd app, says classis is not supported by IOS. They recommend we use the wifi module as a hotspot to transfer this data to the phone and or the cloud. We have 2 months to get this product ready for show and I am at a loss on how to configure and use the module as a hot spot? Any help would be appreciated.