First Time Connection SPWF04SA - Faild ,please help
Hello running the example code : WIFI_Example_Client_Socket
using SPWF04SA
also the server program in the st utility ip 10.0.0.1 (checked with external socket.exe and worekd)
but the WIFI_Example_Client_Socket moo working or sending data please view the log...
/********************************************************
* *
* X-CUBE-WIFI1 Expansion Software v3.1.0 *
* X-NUCLEO-IDW0xx1 Wi-Fi Configuration. *
* Client-Socket Example *
* *
*******************************************************/
Do you want to setup SSID?(y/n):y
Enter the SSID:
yaniv
Enter the password:
magic111
Enter the encryption mode(0:Open, 1:WEP, 2:WPA2/WPA2-Personal):
2
Enter the Hostname (Apache Server):
10.0.0.1
/**************************************************************
* Configuration Complete *
* Port Number:32000, Protocol: TCP/IP *
* Please make sure a server is listening at given hostname *
*************************************************************/
Initializing the wifi module...
Build Configuration:
Nucleo: NUCLEO-L476RG
X-Nucleo: X-NUCLEO-IDW04A1
Interface: UART
with the flowing setup :
then when it freeze / stoped