2023-04-18 07:02 AM
Does STM32 have built-in EtherCAT slave controller?
If it is built in, please tell me the model name。 STM32**
If it is not built in "
What EtherCAT slave controller do you recommend?
2023-04-19 07:23 AM
Hello 清�?暮.1,
You may need to check this firmware STSW-ETHDRV01V1 - Firmware for Servo Drive solution enabling position control through Ethercat Protocol - STMicroelectronics running on the STM32F767ZI microcontroller.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.