cancel
Showing results for 
Search instead for 
Did you mean: 

Connecting SPWF01SA to hidden SSID

Luca DC
Associate II
Posted on September 05, 2017 at 10:47

Hi,

I need to have a SPWF01SA module connect to a Wi-Fi router with hidden SSID.

The first operation the module tries upon starting is '+WIND:21:WiFi Scanning' which completes with the result '+WIND:35:WiFi Scan Complete (0x0)' so the handshake can't proceed.

The module is already fully configured with SSID, password, DNS and so on. It connects successfully as soon as the SSID is made visible.

How can I overcome the void scanning at the beginning and force the connection?

Thank you for your help.

#spwf01sa
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Gerardo GALLUCCI
ST Employee
Posted on October 29, 2017 at 13:37

Use latest FW 3.5.3.

Then, use wifi_region (default: 1; set >= 2) variable to allow module to perform an active scan, and find hidden AP.

By default, module will not perform an active scan into channels where there is no activity.

Posted on December 21, 2017 at 10:29

Even with the latest firmware, module not connects with hidden AP

Posted on December 21, 2017 at 10:29

Tested with all possible values to wifi_region, even not connecting

Posted on December 21, 2017 at 10:31

Firmware version is SPWF02S-170111-665d284-RELEASE-main.bin

Posted on December 21, 2017 at 10:45

Version Misspelled

Correct Firmware version is SPWF01S-170111-665d284-RELEASE-main.bin

And Not connecting to hidden SSID with region_values (1,2,3,4,5,6,7)