2019-08-25 11:43 AM
If I use the timings that are calculated in the "GET_Master_Slave_device_connection_parameters" if I try to connect to slave device error message 0x12. Can I see a correct example of settings for multiple connection?
2019-08-26 6:53 PM
Please refer to documents
file:///C:/Program%20Files%20(x86)/STMicroelectronics/BlueNRG-1_2%20DK%203.1.0/Docs/Multiple_Connection_Guidelines/Multiple_Connection_Guidelines.html
file:///C:/Program%20Files%20(x86)/STMicroelectronics/BlueNRG-1_2%20DK%203.1.0/Docs/Multiple_Connection_Formula/Multiple_Connections_Formula.html
A Multiple Connection Formula Timings Chart spreadsheet is provided for you to emulate the formula calculation and to determine the multiple connections parameters values for your specific application scenario:
file:///C:/Program%20Files%20(x86)/STMicroelectronics/BlueNRG-1_2%20DK%203.1.0/Docs/Multiple_Connection_Formula/Multiple_Connection_Formula_Timings_Chart.xlsx
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.