Skip to main content
rushd
Visitor II
January 28, 2015
Question

BlueNRG support for multiple GAP roles simultaneously

  • January 28, 2015
  • 1 reply
  • 568 views
Posted on January 28, 2015 at 23:22

Hello, I have few questions:

1. Can BlueNRG or BlueNRG MS function as a Central and peripheral role at the same time?

2. Can BlueNRG or BlueNRG MS function as a Central and broadcaster role simultaneously?

3. Can a BlueNRG central device perform discovery of new peripheral devices while connected to 3 other peripheral devices? 

Thanks.

#bluenrg
This topic has been closed for replies.

1 reply

marchese.graziella
Visitor II
March 17, 2015
Posted on March 17, 2015 at 15:11

Hi,

using the  BlueNRG-MS, you can configure all roles (Peripheral|Broadcaster|Central|Observer), while using the BlueNRG you can configure only one role between Peripheral, Broadcaster, Central and  Observer.

Using the BlueNRG device, you cannot perform a discovery procedure while the device is already connected with other devices.

Regards,

Graziella

Hello, I have few questions:

1. Can BlueNRG or BlueNRG MS function as a Central and peripheral role at the same time?

2. Can BlueNRG or BlueNRG MS function as a Central and broadcaster role simultaneously?

3. Can a BlueNRG central device perform discovery of new peripheral devices while connected to 3 other peripheral devices? 

Thanks.