cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG-M2SA body marking reading and how to read the MAC address?

jason239955_st
Associate III
 
1 REPLY 1
Sebastien DENOUAL
ST Employee

Hi @jason239955_st​ ,

 BlueNRG-M2SA is a module based on BlueNRG-2 SoC and so s=you can rely on BleuNRG-2 documentation.

Details on MAC address could be found in PM0269 ( BLE Stack Programming manual) section 3.1.1.

The MAC address is stored in a dedicated place in NVM section managed by BLE stack.

You can use private, public or static random address. The static random address is generated and programmed at first boot of the device on the dedicated Flash are and never erased (except if you perform mass erase)

More details on MAC addresses are available in PM0269 ( BLE Stack Programming manual) section 3.1.1.

Regards,

Sebastien.