cancel
Showing results for 
Search instead for 
Did you mean: 

bluenrg 6.4 update - which file to use

dimitar
Associate II
Posted on January 08, 2015 at 23:25

Hi, 

I have a STEVAL-IDB002V1.

Which image file to use to update the BlueNRG stack to 6.4. 

bluenrg_6_4_Mode_2-16MHz-XO32K. img 

or

bluenrg_6_4_Mode_2-16MHz-XO32K_HCI.img

What is the difference between them?

Thanks
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Scott Löhr
Senior II
Posted on January 09, 2015 at 18:46

I thought that I understood the ST documentation to describe that the *_HCI.img builds (e.g. bluenrg_6_4_Mode_2-16MHz-XO32K_HCI.img) as being built to support ONLY the officially specified HCI commands (i.e. no vendor specific ACI) in order to be used for conformance testing.

Posted on January 21, 2015 at 16:26

Hi Dimitar,

to update the BlueNRG stack to version 6.4 you have to use the firmware image  ''bluenrg_6_4_Mode_2-16MHz-XO32K.img'', in fact as Code has said, the version *_HCI.img  supports only the HCI APIs (no GAP APIs)  and it is provided only for certification.

Regards,

Graziella

Hi, 

I have a STEVAL-IDB002V1.

Which image file to use to update the BlueNRG stack to 6.4. 

bluenrg_6_4_Mode_2-16MHz-XO32K. img 

or

bluenrg_6_4_Mode_2-16MHz-XO32K_HCI.img

What is the difference between them?

Thanks