cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG-2 SPI driver to access LSM6DS3 using direct register access methodology ?

vikrant more
Associate II
Posted on May 28, 2018 at 12:58

I want to access LSM6DS3 sensor which is present on STEVAL-IDB00BV2 board, using direct register methodology (no interrupt )

I tried to initialize SPI as follow. Am I on right track ?

void spi_init()

{

      CKGEN_SOC->CLOCK_EN |= (1 << 4);  //SPI module clock enable

    

      CLRB(SPI->CR1, 1); // SPI disable ....(as per 3.8.2.2 point mentioned in Datasheet of BlueNRG_2)

  

      GPIO->MODE0 = 0;

      GPIO->MODE0 |= 0x00004444; // IO0, IO1, IO2, IO3 set to mode serial0

    

      GPIO->OEN |= 0x00000007;

      CLRB(GPIO->OEN, 3);

      SETB(GPIO->PE, 3);

      SPI->CPSR |= 0x00000004;

    

      SPI->CR0 = 0x00000447; // 8-bit data, Steady-state of clock polarity is high, Steady-state of clock phase is low

                                                 // the slave 1 is selected, SCR = 4, Motorola SPI frame format, Full duplex mode

                                                 //

      SPI->CR1 = 0x00000000; // Master mode,

    SETB(SPI->CR1, 1);  // SPI enable

}

Now how to access, WHO_AM_I register (addr -> 0x0F ....for reading it should OR with 0x80) ?

Thank You !!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0