cancel
Showing results for 
Search instead for 
Did you mean: 

请问BLUENRG1能够输出两路�?�控制的PWM�?�?

WYao.1
Associate

请问BLUENRG1能够输出两路�?�控制的PWM�?�?最好是能够控制PWM的开�?�关闭,PWM的�?�空比。我�?试�?作定时器在工作模�?1和1a下工作,Txen都无法控制输出的开�?�关闭,是�?作方法�?对�?�?

1 REPLY 1
Winfred LU
ST Employee

Yes. Two PWM sources (PWM0 and PWM1) can be configured independently.

Please refer to MFT/PWM_SW sample in DK.