2020-07-24 1:35 PM
I have a single 'known good' VL53L0X hooked up to an Arduino Mega 2560 through a bidirectional level shifter. When I attempt to initialize it I get the following output:
Opening port
Port open
Arduino Hex VL53L0X Demo
In Adafruit_VL53L0X::begin(29,1,642)
VL53L0X Info:
Device Name: VL53L0X ES1 or later, Type: VL53L0X, ID: VL53L0CBV0DH/1$1
Rev Major: 1, Minor: 1
VL53L0X: StaticInit
VL53L0X: PerformRefSpadManagement
refSpadCount = 2226323456, isApertureSpads = 10
Status = -6
VL53L0X Error: -6
Failed to boot lidar_RFIt looks like the I2C bus is OK, as it is reading the device name and details correctly, but the VL53L0X_PerformRefSpadManagement() call returns with Status = -6, and the rest of the initialization is skipped.
I tried modifying the library code to skip the VL53L0X_PerformRefSpadManagement() call, but then VL53L0X_PerformRefCalibration() also returns with a -6 Status code.
Any idea what I'm doing wrong here?
TIA,
Frank
2020-07-24 4:12 PM
Is it possible that you did not call DataInit() prior to calling StaticInit()?
"VL53L0X_DataInit() function is called one time, and it performs the device initialization.
To be called once and only once after device is brought out of reset."
It sets a bunch of registers into a more optimal state before the chip gets going.
I've seen this error before, but the customer found his bug and did not tell me what he changed.
But you did a good job of showing me what you called, and I did not see DataInit().
2020-07-24 7:14 PM
John,
Thanks for the prompt reply. I'm using the Adafruit library, and I believe all the setup code is in their begin() function, as follows:
/**************************************************************************/
boolean Adafruit_VL53L0X::begin(uint8_t i2c_addr, boolean debug, TwoWire *i2c) {
uint32_t refSpadCount;
uint8_t isApertureSpads;
uint8_t VhvSettings;
uint8_t PhaseCal;
//DEBUG!!
Serial.print("In Adafruit_VL53L0X::begin(");
Serial.print(i2c_addr,HEX); Serial.print(",");
Serial.print(debug); Serial.print(",");
Serial.print((uint16_t)i2c,HEX); Serial.println(")");
//DEBUG!!
// Initialize Comms
pMyDevice->I2cDevAddr = VL53L0X_I2C_ADDR; // default
pMyDevice->comms_type = 1;
pMyDevice->comms_speed_khz = 400;
pMyDevice->i2c = i2c;
pMyDevice->i2c->begin(); // VL53L0X_i2c_init();
//DEBUG!!
//Serial.println("After pMyDevice->i2c->begin()");
//DEBUG!!
// unclear if this is even needed:
if (VL53L0X_IMPLEMENTATION_VER_MAJOR != VERSION_REQUIRED_MAJOR ||
VL53L0X_IMPLEMENTATION_VER_MINOR != VERSION_REQUIRED_MINOR ||
VL53L0X_IMPLEMENTATION_VER_SUB != VERSION_REQUIRED_BUILD) {
if (debug) {
Serial.println(F(
"Found " STR(VL53L0X_IMPLEMENTATION_VER_MAJOR) "." STR(VL53L0X_IMPLEMENTATION_VER_MINOR) "." STR(
VL53L0X_IMPLEMENTATION_VER_SUB) " rev " STR(VL53L0X_IMPLEMENTATION_VER_REVISION)));
Serial.println(F("Requires " STR(VERSION_REQUIRED_MAJOR) "." STR(
VERSION_REQUIRED_MINOR) "." STR(VERSION_REQUIRED_BUILD)));
}
Status = VL53L0X_ERROR_NOT_SUPPORTED;
return false;
}
Status = VL53L0X_DataInit(&MyDevice); // Data initialization
if (!setAddress(i2c_addr)) {
return false;
}
Status = VL53L0X_GetDeviceInfo(&MyDevice, &DeviceInfo);
if (Status == VL53L0X_ERROR_NONE) {
if (debug) {
Serial.println(F("VL53L0X Info:"));
Serial.print(F("Device Name: "));
Serial.print(DeviceInfo.Name);
Serial.print(F(", Type: "));
Serial.print(DeviceInfo.Type);
Serial.print(F(", ID: "));
Serial.println(DeviceInfo.ProductId);
Serial.print(F("Rev Major: "));
Serial.print(DeviceInfo.ProductRevisionMajor);
Serial.print(F(", Minor: "));
Serial.println(DeviceInfo.ProductRevisionMinor);
}
if ((DeviceInfo.ProductRevisionMajor != 1) ||
(DeviceInfo.ProductRevisionMinor != 1)) {
if (debug) {
Serial.print(F("Error expected cut 1.1 but found "));
Serial.print(DeviceInfo.ProductRevisionMajor);
Serial.print(',');
Serial.println(DeviceInfo.ProductRevisionMinor);
}
Status = VL53L0X_ERROR_NOT_SUPPORTED;
}
}
if (Status == VL53L0X_ERROR_NONE) {
if (debug) {
Serial.println(F("VL53L0X: StaticInit"));
}
Status = VL53L0X_StaticInit(pMyDevice); // Device Initialization
}
if (Status == VL53L0X_ERROR_NONE) {
if (debug) {
Serial.println(F("VL53L0X: PerformRefSpadManagement"));
}
Status = VL53L0X_PerformRefSpadManagement(
pMyDevice, &refSpadCount, &isApertureSpads); // Device Initialization
if (debug) {
Serial.print(F("refSpadCount = "));
Serial.print(refSpadCount);
Serial.print(F(", isApertureSpads = "));
Serial.println(isApertureSpads);
Serial.print(F("Status = ")); Serial.println(Status);
}
}
if (Status == VL53L0X_ERROR_NONE) {
if (debug) {
Serial.println(F("VL53L0X: PerformRefCalibration"));
}
Status = VL53L0X_PerformRefCalibration(pMyDevice, &VhvSettings,
&PhaseCal); // Device Initialization
}
if (Status == VL53L0X_ERROR_NONE) {
// no need to do this when we use VL53L0X_PerformSingleRangingMeasurement
if (debug) {
Serial.println(F("VL53L0X: SetDeviceMode"));
}
Status = VL53L0X_SetDeviceMode(
pMyDevice,
VL53L0X_DEVICEMODE_SINGLE_RANGING); // Setup in single ranging mode
}
// Enable/Disable Sigma and Signal check
if (Status == VL53L0X_ERROR_NONE) {
Status = VL53L0X_SetLimitCheckEnable(
pMyDevice, VL53L0X_CHECKENABLE_SIGMA_FINAL_RANGE, 1);
}
if (Status == VL53L0X_ERROR_NONE) {
Status = VL53L0X_SetLimitCheckEnable(
pMyDevice, VL53L0X_CHECKENABLE_SIGNAL_RATE_FINAL_RANGE, 1);
}
if (Status == VL53L0X_ERROR_NONE) {
Status = VL53L0X_SetLimitCheckEnable(
pMyDevice, VL53L0X_CHECKENABLE_RANGE_IGNORE_THRESHOLD, 1);
}
if (Status == VL53L0X_ERROR_NONE) {
Status = VL53L0X_SetLimitCheckValue(
pMyDevice, VL53L0X_CHECKENABLE_RANGE_IGNORE_THRESHOLD,
(FixPoint1616_t)(1.5 * 0.023 * 65536));
}
if (Status == VL53L0X_ERROR_NONE) {
return true;
} else {
if (debug) {
Serial.print(F("VL53L0X Error: "));
Serial.println(Status);
}
return false;
}
}