Skip to main content
MPate.5
Visitor II
January 9, 2021
Question

VL53L5 TOF Sensor:- Can we use two VL53L5 Sensor on same I2C bus? Can we configure the I2C Address of VL53L5 Sensor ? Where we find the Datasheet of VL53L5 Sensor ?

  • January 9, 2021
  • 2 replies
  • 929 views

..

This topic has been closed for replies.

2 replies

John E KVAM
ST Employee
January 11, 2021

One can put multple VL53 (of any variety) on a single I2C bus.

However as the VL53L5 can return up to 4 targets for each of 64 zones per range, the I2C traffic can get kind of large.

One woud need to use the 1Mbit setting on the I2C and keep the wire length and capacitance well tuned.

As to the datasheet. That'a a harder question.

The part is out and selling well into the cellphone and PC markets.

But before we release it to everyone we still have some work to do.

Our current customers are helping us refine the process so it will be easy for everyone to implement.

You don't need the startup hassles, and there is no way I could support too many customers this way.

The full part should be out by June.

And by then it should be quite simple to integrate.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
Guopeng
Associate II
May 9, 2021

Dear John,

I just want to know what is the plan for this VL53L5, will ST also provide some drivers for STM32, or just for Linux?

And also the timeline is still June 2021?