cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L1X-SATEL / no blocking function

Talex.1
Associate II

I connect a vl53l1x-satel to a stm32wb55rg6 with 4 essantial pins (sda, sdl, gnd, vdd). I have a problem to wait for a result. With de function VL53L1_WaitMeasurementDataReady() i haven't problems but for my project I must not use a blocking function. So I try VL53L1_GetMeasurementDataReady() whitout success. I would like use a physical interrupt but i don't understant it's works and how use it.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
John E KVAM
ST Employee

​It's the job of the sensor to raise the interrupt and the job of the STM32 (and the programmer) to handle it. :)

But let me try to give you some ideas.

First you can try posting your question the STM32 MCU community.

You will get a lot of answers - and perhaps some code.

Another option is to tell the VL53L1x to range continuously and autonomously forever.

Then just read the result whenever you felt like it.

With a 30ms TimingBudget, you might get some data that's 29ms old, or you might get the same data twice, but as new data becomes available you'd get it.

This is how a lot of robots work.

Another idea would be:

The VL53L1_WaitMeasurementDataReady() does a loop

loop forever {

   done = VL53L1_GetMeasurementDataReady()

   if done, exit loop

   wait a bit

{

Simply create a function similar to this and change the "wait a bit" to "do something useful here"

Thirdly - it's always a good idea when looking for technical information to simply "Google it".

I googled "STM32 Interrupt" and got some good articles.

 Don't be thrown off by the mention of ARM Cortex - that's the architecture inside the STM32.

  • good luck
  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.