cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L1CB

labubu
Associate II

VL53L1CB的最低投资回报率配置是 4x4?我可以将其配置为 1x1 吗?

Translated : The minimum ROI configuration for the VL53L1CB is 4x4? Can I configure it as 1x1?

1 ACCEPTED SOLUTION

Accepted Solutions
John_Kvam
Senior II

A 4x4 region of interest is about the limit. Each photon strike needs a quench cycle to reset the detector. Any fewer than 16 and it would take forever to get enough photons to get a measurement. 

So, alas, 4x4 is the minimum.

It also insures there is enough flexibility for the sensor to adjust the SPADs (detectors.) Not all of them are the same. 

- john 

 

If this or any post solves your issue, please mark them as "Accept as Solution". It really helps the next guy.
And if you notice anything wrong do not hesitate to "Report Inappropriate Content".
I am a recently retired ST Employee. My former username was John E KVAM.

View solution in original post

1 REPLY 1
John_Kvam
Senior II

A 4x4 region of interest is about the limit. Each photon strike needs a quench cycle to reset the detector. Any fewer than 16 and it would take forever to get enough photons to get a measurement. 

So, alas, 4x4 is the minimum.

It also insures there is enough flexibility for the sensor to adjust the SPADs (detectors.) Not all of them are the same. 

- john 

 

If this or any post solves your issue, please mark them as "Accept as Solution". It really helps the next guy.
And if you notice anything wrong do not hesitate to "Report Inappropriate Content".
I am a recently retired ST Employee. My former username was John E KVAM.