2019-04-10 5:00 PM
Everywhere I look, the VL53L1X Tof Sensor says that it has a standard fov of 27 degrees (or 16x16) and can be reduced to 15 degrees (or 4x4 SPAD array). But how do I do this on the Raspberry Pi (in python)? In your VL53L1X_register_map.h there is a function called:
#define VL53L1_ROI_CONFIG__MODE_ROI_XY_SIZE 0x013F
/*!<
type: uint8_t \n
default: 0x00 \n
info: \n
- msb = 7
- lsb = 0
- i2c_size = 1
groups: \n
['nvm_copy_data', 'roi_config']
fields: \n
- [7:0] = mode_roi_xy_size
*/How do I use this or another function to make my ROI 15 degrees (4x4 SPAD) instead of 27 on the Raspberry Pi like your documentation says it can? Or do I have to hook it up to some software and do it in there to change it?
2019-04-16 8:23 AM
Quickly download the UltraLitte driver from ST.com - STSW-IMG009.
The code in here is very simple. You can use that as an example.