cancel
Showing results for 
Search instead for 
Did you mean: 

I am using VL53L1X ToF sensor. I am able to use Short and Long Distance modes but How can I configure the sensor to medium mode ?

GL.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Julien NGUYEN
ST Employee

Hi,

What is the driver are using ? Actually we do have two version of the driver for the VL53L1X, stsw-img007 and stsw-img009. The 009 has only 2 distance modes, We did not implement the medium mode in this driver because there is no any benefit. The short mode has better ambient immunity but the max distance measurable is shorter while the long distance mode has a longer max distance measurable but less performant in ambient light.

Thanks

Julien


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
GL.1
Associate

Hi,

The driver I am using is STSW-IMG010.

As we are using VL53L1X, we want to test the sensor in medium mode. Can you suggest driver that contains all the features (3 Distance modes, Interrupt), so that it will be useful for our project

Thanks,

Gayathri