cancel
Showing results for 
Search instead for 
Did you mean: 

Getting timestamps from STEVAL-EVK-U0I boards

oaa3wf
Associate II

Hi, 

Is it possible to get some sort of frame timestamp from the evaluation boards? Ideally, I would love to have start and end of exposure timestamps but any timestamp from the sensor would be great. I could timestamp when I receive the frame on my device, but that might not be accurate enough for my application since it would also include other delays from my computer. Inaccuracies in the 10s of microseconds range are acceptable.

 

Thanks.

1 ACCEPTED SOLUTION

Accepted Solutions
michaeltang
ST Employee

Hello @oaa3wf,

The evaluation board itself did not measure the exact timing of exposure envelop. But there's "STROBE" signal from GPIO config register you may use to monitor the exposure from your host.

You may use a STM32 to capture this signal by a GPIO interrupt and get the timestamp from ISR (like the `STM32HAL_GetTick()` mentioned by John)


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
John_Kvam
Senior II

This is really an STM32 question. And that sensor does have a way to convert clock cycles to milliseconds.

I did post long ago on how to do it, but when I retired I kind of lost all my example code. 

Do a bit of Googling and look for STM32HAL_GetTick()

That should get you to some code that does what you want. 

- john (ST 'graduate' of the Imaging Group - and proudly so.)

 

If this or any post solves your issue, please mark them as "Accept as Solution". It really helps the next guy.
And if you notice anything wrong do not hesitate to "Report Inappropriate Content".
I am a recently retired ST Employee. My former username was John E KVAM.
michaeltang
ST Employee

Hello @oaa3wf,

The evaluation board itself did not measure the exact timing of exposure envelop. But there's "STROBE" signal from GPIO config register you may use to monitor the exposure from your host.

You may use a STM32 to capture this signal by a GPIO interrupt and get the timestamp from ISR (like the `STM32HAL_GetTick()` mentioned by John)


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @michaeltang and @John_Kvam , I was finally able to test this and could read the strobe signal, thanks. Do you know if/how the strobe signal output from one STEVAL-EVK-U0I board could be used to control the frame capture on another STEVAL-EVK-U0I board? I've read the document: um2602-how-to-integrate-and-configure-the-vd56g3-vd66gy-and-vd16gz-devices-from-a-hardware-and-software-perspective-stmicroelectronics.pdf  , but it is still not clear to be if the strobe signal is output only.