2021-05-13 01:33 PM
I have a Teseo LIV3R on a breakout board connected (via UART) to Tesio Suite. I'm trying to figure out how to enable STAGPS and test its functionality. Unfortunately I cannot enable the autonomous STAGPS engine using the command:
$PSTMSTAGPSONOFF,1
When sending the command $PSTMSTAGPSONOFF,1 to the module, I get no response. I would expect a response such as $PSTMPOLSTARTED. When sending the command $PSTMCFGAGPS,1 I get a response that the AGPS engine has been enabled. I would like to enable the autonomous STAGPS functionality though but I am not able to.
Hopefully someone canhelp or have an idea what the problem is?
Also, I was not able to confirm if the autonomous STAGPS function is enabled as default. Does anyone know if it is, and how to confirm this?
Thanks in advance.
2021-05-14 08:01 AM
Hi
ST-AGPS is enabled by default in LIV3R.
Regards
Francesco
2021-05-18 04:46 AM
Thanks Francesco, do you know how I can verify that as well as switch on/off this feature?
I had no luck using $PSTMSTAGPSONOFF,1 and $PSTMSTAGPSONOFF,0
Thanks,
Martin.