| Subject | Author | Posted | |
|---|---|---|---|
|
Hi, I'm trying to configure DIO1 and DIO0 as outputs in my custom board, but I can't get them to w...
| 2025-05-25 1:52 PM | ||
|
Hello, I'm using STEVAL-IDB011V2. From the BlueNRG-LP Navigator, I can load the examples on the...
| 2025-05-19 8:43 PM | ||
|
We found that the BlueNRG component is not connecting with the ST BLE Drone App. We have verified ...
| 2025-04-24 2:33 AM | ||
|
We are interns, and as part of our internship project, we tried to create a replica of the STEVAL-F...
| 2025-04-24 2:24 AM | ||
|
Hi.
I am using two STPM34 on my board, they are separated, UART, SCS, SYN, all of them. I got ini...
| 2025-04-04 4:55 AM | ||
|
platform:BLUENRG345_MC SDK :BLUENRG_LP_1.2.0 Our device serves as a broadcaster (directional broa...
| 2025-04-03 1:42 AM | ||
|
Hello everyone Do you know where can I find a ready to use example for X-NUCLEO-S2915A1 . It seems...
| 2025-03-31 11:04 AM | ||
|
Hallo, I have in my middlewares BluNRG2 packet. I have this function aci_gatt_add_char that adds a...
| 2025-03-31 9:37 AM | ||
|
Hi, I've been struggling with this for 2 weeks now so I'm reaching out desperate for help. Our cu...
| 2025-03-26 9:24 AM | ||
|
I have configured the hardware to use BlueNRG-M2SA(DIO4, DIO5) with STM32L053R8T6 via LPUART1(PB10,...
| 2025-03-25 7:07 PM | ||
|
Hi Everyone, I'm using STM32L4 microcontroller to communicate with BlueNRG-MS over SPI. I'm tryi...
| 2025-03-19 1:37 PM | ||
|
Hello, I am trying to evaluate S2-LP. I have tried a couple of example codes to make one device se...
| 2025-03-19 12:11 AM | ||
|
Hi,
I am looking for an LPAd (Local Profile Assistant - Device) for Linux to manage eSIM profiles...
| 2025-03-14 2:52 AM | ||
|
Edit by ST Moderator: This post has been translated from French to comply with the ST Community Ter...
| 2025-03-12 2:26 PM | ||
|
Hello, I am currently experiencing issues with my S2LP. When I start it, I switch it directly to S...
| 2025-03-12 2:52 AM | ||
|
We use STM32L162xx MCU to communicate with S2_LP and SP_BTLE drivers via SPI.
With S2-LP, it ...
| 2025-03-07 1:59 AM | ||
|
I am using STM32L34 with STPM34, where I am trying to disable CRC once the power up sequence is don...
| 2025-02-25 12:45 AM | ||
|
Hi, I am using a SIM7080G module along with the eSIM model ST4SI2M0020TPIFW, and when I use the AT...
| 2025-02-24 1:18 PM | ||
|
Dear all, Im currently using STSW-IOL4LSV1 package for evaluation. My Company has no IO-Link ven...
| 2025-02-17 2:17 PM | ||
|
Hi everyone, I am developping an application on the BlueNRG-M2SA module (BLE 4.2) supporting Multi...
| 2025-02-03 1:38 AM |