Subject | Author | Posted | |
---|---|---|---|
In some training session they are using ADC calibration in the code , whether it is required ? An...
| 2021-11-17 06:58 AM | ||
I am currently using the HAL function ``` HAL_I2S_Receive (I2S_HandleTypeDef * hi2s, uint16_t * ...
| 2021-11-02 08:29 PM | ||
TDA7577, PIN16 pin is left floating to disable I2C bus mode, the speaker short-circuit fault is d...
| 2021-10-31 12:33 AM | ||
Already i worked in asc ml program but there are some delay to find the word using asc so give some...
| 2021-10-26 04:46 AM | ||
How to configure ADC in STEVAL - MKSBOX1v1 (With DMA or W/o DMA) How are the setting to be used f...
| 2021-10-20 08:12 AM | ||
I have tried a few power/ground schemes, series resistance on the ABC lines, etc. Nothing lowers t...
| 2021-10-06 12:12 PM | ||
2021-10-04 01:32 AM | |||
which product category is ldk120, sot323 in this table . needed for compliance documentation
| 2021-09-20 02:18 AM | ||
2021-09-16 06:19 AM | |||
2021-09-14 03:54 AM | |||
2021-09-12 07:42 AM | |||
I have been using STEVAL-IKR002V4D (a daughterboard with SPIRIT1 868 Mhz transceiver) to transmit d...
| 2021-09-06 09:35 PM | ||
Hi, How to set STA311 for 2.1 by APWorkbench? for example, ch1 and ch2 mix to ch6 output.
| 2021-09-01 11:33 PM | ||
I use the Bluecoin starter kit to steam the audio by STSW-BCNKT01 software. when using the micro-U...
| 2021-08-16 12:54 AM | ||
Hi, I am using FP-AUD-BVLINK2 pack on Bluecoin. I want integrate fp-aud-smartmic1 Beamforming Ac...
| 2021-08-11 09:02 AM | ||
part # 09395699 delco ic. can you give me your part # It is a st part.
| 2021-07-29 09:36 AM | ||
2021-07-24 12:03 AM | |||
We want to utilize the diode STTH3003. It would be great to have some information about the dielect...
| 2021-07-21 06:30 AM | ||
Hello! I want to ask you some advice in building a class D amplifier using the integrated circuit ...
| 2021-06-29 10:17 AM | ||
2021-06-24 03:52 AM |