| Subject | Author | Posted | |
|---|---|---|---|
|
Hi All, I have custom phycore stm32mp13 based carrier board and i want to create uboot splash scre...
| 2024-12-01 10:56 AM | ||
|
Hello, I run make for install USB wifi driver for STM32MP1. I had import enviroment, but i can't m...
| 2024-11-27 1:31 AM | ||
|
Hi All, I am working on enabling and testing the LCD (RGB666) and backlight (enable and pwm) funct...
| 2024-11-24 2:03 PM | ||
|
Hi there, I am working on a product where we use the STM32MP157C for our purposes At the moment w...
| 2024-11-22 4:33 AM | ||
|
Hi, We are wondering that do we support to boot uboot from nand flash then boot into OS from exter...
| 2024-11-21 7:39 PM | ||
|
Hello: I am debugging the network development of STM32MP135 bare metal, using the protocol stack...
| 2024-11-21 9:04 AM | ||
|
We are using STM32MP!57A processor in our custom board. In this we are unable to read t...
| 2024-11-20 5:52 AM | ||
|
Hello, I have a STM32MP2 platform with A/B partitioning for TF-A, metadata and FIP. I'm looking f...
| 2024-11-18 6:30 AM | ||
|
Hello! If I run the openAMP example I can see the two new devices appear in the linux /dev folder:...
| 2024-11-12 5:08 AM | ||
|
Hello, We are evaluating the X-STM32MP-GNSS1 eval board on STM32MP-157F-DK2. The X-STM32MP-GNS...
| 2024-11-12 3:33 AM | ||
|
I'm working with the STM32MP131FAE in a bare-metal environment, and I'm experiencing issues ...
| 2024-11-11 2:19 AM | ||
|
Hello, I am developing on the STM32MP131FAE board in a bare-metal environment. This chip does not...
| 2024-10-30 10:20 PM | ||
|
Description: I'm working with the MYIR MYD-YA157C board, based on the STM32MP157C, and experiencing...
| 2024-10-26 3:07 AM | ||
|
I am trying to connect to audio codecs to give 4 channel of audio on a MP257. Can I connect SAI2.SC...
| 2024-10-23 7:52 AM | ||
|
I am getting an error when working through the README.HOW_TO.txt in linux-stm32mp-6.1.82-stm32mp-r2...
| 2024-10-22 8:19 PM | ||
|
I have started working on STM32MP257f board. I have installed open st linux distribution package on...
| 2024-10-20 11:56 PM | ||
|
Hello, I am using meta-st-stm32mp which points to mickledore and is using linux 6.1.82. I woul...
| 2024-10-07 1:56 AM | ||
|
How can I enable the HDMI output log at boot? I want to see the login promt at the HDMI output.
| 2024-10-02 3:30 PM | ||
|
I want to display the loop log at start up from UART to the HDMI. How can i achieve that? Is it so...
| 2024-09-29 2:09 PM | ||
|
Hello everyone, we have developed a custom board based on stm32mp157 chip. We have also forked the...
| 2024-09-18 8:25 AM |