| Subject | Author | Posted | |
|---|---|---|---|
|
Hi, hope you doing good. We are currently using NUCLEO-L412RB-P along with X-NUCLEO-60K1A1 for te...
| 2026-02-12 7:41 AM | ||
|
Found a bug with RX_POOL buffers been permanently used. There are total of 12 buffers defined by de...
| 2026-02-10 8:42 AM | ||
|
I am working with a custom board that uses the STM32H7S38T chip.
I am trying to use the SPI flash...
| 2026-02-10 7:01 AM | ||
|
Board: NUCLEO-N657X0-Q, revision C I'm trying to communicate with an I2C sensor (VL53L7CX) using t...
| 2026-02-08 10:55 AM | ||
|
Expected Log using UART : [BOOT] UART initialized successfully [BOOT] Starting ThreadX ke...
| 2026-02-03 6:02 AM | ||
|
Hello everyone, I'm having some trouble implementing I3C communication and would like to ask for so...
| 2026-01-29 11:15 PM | ||
|
Hi team,
I am working with the STM32H7S78-DK board and implementing TLS 1.3 using WolfSSL on the ...
| 2026-01-17 6:23 AM | ||
|
Hello, I am looking for help debugging an issue with both ADCs running in continuous conversion mo...
| 2026-01-03 2:56 AM | ||
|
Hi everyone, I'm using the NUCLEO-H7S3L8 to try to comunicate with a BOS1921 device using the I...
| 2025-12-21 7:48 AM | ||
|
Hello there, as wolfssl_connect is not getting out any ClientHello, I was wondering if it is d...
| 2025-12-17 8:50 PM | ||
|
Hello ST! This is a bug report of sorts, since the `UTIL_SEQ_Run()` function is still marked that ...
| 2025-12-17 5:56 AM | ||
|
Hi, I have been using OpenAMP on an STM32H755ZIT MCU recently but ran into an issue where the mc...
| 2025-12-16 8:03 AM | ||
|
Hi, I'm trying to implement a simple tickless idle on my STM32H7 running on the CM7 core i use TIM...
| 2025-12-10 3:58 PM | ||
|
Hello ST Team, I'm implementing robust Ethernet on STM32H743ZI. Need technical guidance on: PART ...
| 2025-12-10 4:05 AM | ||
|
We use STM32H743 to develop a system that needs to display a 1920 * 1080(8-bit pixel depths) graphi...
| 2025-12-08 9:39 AM | ||
|
Post edited by ST moderator to be inline with the community rules for the code sharing. In next tim...
| 2025-12-08 4:12 AM | ||
|
Hello
Yes here we go again… I’m again busy with the implementation of PTP slave inside STM32H7, b...
| 2025-11-28 11:06 AM | ||
|
Reply to you How to fix SDIO error HAL_SD_ERROR_RX_OVERRUN? - STMicroelectronics Community ...
| 2025-11-22 4:40 PM | ||
|
I have been trying for a while now to do something simular to this with threadx https://community....
| 2025-11-19 12:05 PM | ||
|
STM32 MCUs hide surprisingly useful hardware features that can save you CPU cycles, lower power, ma...
| 2025-11-17 1:37 PM |