| Subject | Author | Posted | |
|---|---|---|---|
|
wondering what these pins do as the shutter goes to the 1v5 regulator input and the flash comes fro...
| 2024-08-23 7:06 PM | ||
|
I am doing research to test the performance of an MCU based system that transports the raw PC...
| 2024-08-23 10:09 AM | ||
|
All: I have the IDB00BV2 and am using the Keil Uvision_5 tool with the compiler back leveled to ve...
| 2024-08-20 9:17 AM | ||
|
Hi everyone, I’m working on a project that requires developing a driver for the Goodix GT2931 capa...
| 2024-08-14 10:05 AM | ||
|
I create project with CubeMX, use Keil MDK IDE, CM7 core without user code , CM4 core has simple us...
| 2024-08-05 9:38 PM | ||
|
I am using the B-l4s5i -iot01 board to test connecting to the AWS platform. I started from FP-CLD-A...
| 2024-08-01 12:48 PM | ||
|
hello. My name is Kim and I work for a company in Korea.
I have been trying to purchase ST-LI...
| 2024-07-18 12:50 AM | ||
|
Hello, I have an STM32H7S78 development kit and I am new to using it. On this board, I have tried s...
| 2024-07-11 12:19 AM | ||
|
Hello STM32 Community, I have the STM32F413ZH Discovery Kit, which comes with a 240x240 TFT displa...
| 2024-07-05 12:02 AM | ||
|
Hello everybody I'm using stm32f401re bord to read nfc08a1 data but the nfc08a1 not providedin...
| 2024-06-26 1:16 PM | ||
|
Hello forum I want to make a code that saves pictures from the camera module into an external SD...
| 2024-06-26 3:56 AM | ||
|
Hello Team, I encountered an issue while using the ST-LINK GDB server version 7.6.0. The server st...
| 2024-06-25 3:28 AM | ||
|
Hello everyone I've being trying to setup a DAC output using DMA in a nucleo U575ZI-Q board.I s...
| 2024-06-14 6:56 AM | ||
|
Hello, my problem is as follows:I did a chip regression with flash erase and now I cannot conne...
| 2024-06-10 2:28 AM | ||
|
Hello, I am using the P-L496AG-CELL02 board and am creating a program to read the value of ADC1 at...
| 2024-06-07 6:51 AM | ||
|
Hey there, I'm a first-time user of the STM32 and I'm using the STM32F103C8T6 (Bluepill Board)....
| 2024-06-03 3:03 AM | ||
|
Hello! I'm using Amicam1 module with stm32L476RG. I've reworked the default example and enabled si...
| 2024-05-30 12:46 PM | ||
|
Hello everyone, There are 24pcs WS2813-Mini led on my PCB. I didn't set these with timer. How c...
| 2024-05-29 2:49 AM |