cancel
Showing results for 
Search instead for 
Did you mean: 

XCUBE-AI Keras model Analysis/Validation error.

MQabb.1
Associate

I have encountered error while executing validation on my first Keras model using XCUBE.AI extension. The error message below,

----------------------------------------------------------------------------------------------------------------------------------

Analyzing model 

Neural Network Tools for STM32 v1.2.0 (AI tools v5.0.0) 

TOOL ERROR: Traceback (most recent call last): 

  File "C:\Users\moham\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.0.0\Utilities\windows\tensorflow_core\python\pywrap_tensorflow.py", line 58, in <module> 

    from tensorflow.python.pywrap_tensorflow_internal import * 

  File "C:\Users\moham\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.0.0\Utilities\windows\tensorflow_core\python\pywrap_tensorflow_internal.py", line 28, in <module> 

    _pywrap_tensorflow_internal = swig_import_helper() 

  File "C:\Users\moham\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\5.0.0\Utilities\windows\tensorflow_core\python\pywrap_tensorflow_internal.py", line 24, in swig_import_helper 

    _mod = imp.load_module('_pywrap_tensorflow_internal', fp, pathname, description) 

  File "imp.py", line 242, in load_module 

  File "imp.py", line 342, in load_dynamic 

ImportError: DLL load failed: A dynamic link library (DLL) initialization routine failed. 

Failed to load the native TensorFlow runtime. 

See https://www.tensorflow.org/install/errors 

for some common reasons and solutions.  Include the entire stack trace 

above this error message when asking for help.

----------------------------------------------------------------------------------------------------------------------------------

I'm using

STMCubeMx version 5.6.1

XCUBE.AI version 5.0.0

I installed "microsoft Visual C++ 2015,2017,2019 Redistributable Update 3" as recommended in another thread.

Could you please support as I'm stuck with this error for 3 days now?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
fauvarque.daniel
ST Employee

Are you on Windows 10 ? our generation machine is on Windows 10 and we don't support Windows 7 anymore.

Regards

Daniel

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi Daniel,

​

​T​hanks for your reply.

​

Y​es I'm using Windows 10.

fauvarque.daniel
ST Employee

According to this thread it is as you said a question of C++ redistributable version

In one comment is says: " please uninstall the latest Microsoft Visual C++ Redistributable for Visual Studio version if you install 2019 and before that

download Microsoft Visual C++ Redistributable for Visual Studio 2015, 2017 and 2019 depending on your system either x64 or x86 on this website

https://support.microsoft.com/en-my/help/2977003/the-latest-supported-visual-c-downloads"

I wonder if it could also be some non English Windows issues, is your Windows in English ?

Sorry for not being of better help I have never seen this issue on our machines

Regards

Daniel

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.